ACM Default Settings

How do I open ACM Default Settings?
  • From the
    TOOLS
    menu, select
    Settings
    .
Use
ACM Default Settings
to specify the location of the system file, the language shown in the display, how ControlLogix content is generated, and whether to show indications.
Setting
Description
System Documentation Path
The location of the template files. By default the files are in
C:\Users\Public\Documents\Studio 5000\Templates\
Application Code Manager
\(RA-TPL) ACM 2.00
.
Language
The language used by
Application Code Manager
. The default value uses the operating system language.
Auto-expand Preview when adding new content
Determines whether the tree in
Preview
is automatically expanded. The default value is selected.
Controller Generation Defaults
Determines what is selected to include in Logix code generated by ACM and whether
Application Code Manager
should overwrite existing output with new code.
Overwrite Existing Output
The default setting for
Overwrite Existing
in the
Logix Code Generation
window.
ACM Project Data
The default setting for
ACM Project Data
in the
Logix Code Generation
window.
Create ACD
The default setting for
Create ACD
in the
Logix Code Generation
window.
Show ACD Warnings
Determines whether the
Status
column in the
Logix Code Generation
window shows ACD warnings. Find the warnings in the log file.
Determines whether indications are shown.
Modified Objects
Sets whether an indication is shown when a library object has been modified. The default value is cleared.
Newer Library Version Available
Sets whether an indication is shown when a node or folder contains one or more libraries that has a newer version available in
Registered Libraries
. The default value is cleared.
Library Export Options
Configures the exported files, includes:
  • Exclude revision number from file name
    : remove the revision number from the exported files. The
    Highest revision library only
    option will be selected automatically after selecting this option.
  • Highest revision library only
    : export the highest revision library only.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal