Add content to an ACD project
Add content from the ACM library to an existing ACD project by opening the ACD in
Application Code Manager
.To add ACM library content to an ACD project
- ClickTOOLSand clickOpen Target ACD.
- Select the desired ACD file, and then clickOpen.
- TheTarget ACD Filetab will replace thePreviewpane.
- Drag and drop content from the registered libraries or an existing ACM project to theTarget ACD Filetab. TheTarget ACD Generation Wizard - Object Configurationpage appears.TIP:Click theOverride Calculated Parametersbutton to unlock the calculated parameter of this object. The unlocked calculated parameter can be edited. After editing, click theEnforce Calculated Parametersbutton to lock this parameter.
- (optional) ClickOPTIONS > Include Project Datato include all instances with their parameter values, as well as all libraries (zipped) will be included as part of the Controller's Custom Properties.
- Resolve any values in theUnresolved Namespage, then clickNext. TheTarget ACD Generation Wizard - Merge Actionspage appears.
- Review the list of merge actions.
- If any merge actions are incorrect, clickBackto update the parameters as needed.
- If the merge actions are correct, clickNext.TheTarget ACD Generation Wizard - L5X Generation Successfulpage appears.
- ClickNext. TheSave Asdialog opens. InFile nameeither:
- Type a name for the ACD file that contains the merged content.
- Leave the original name to overwrite the existing ACD project (default).
- ClickSaveto save the target ACD file.
- ClickFinish.
Provide Feedback