OPCBrowser object
The OPCBrowser object browses item names in the server's configuration. There exists only one instance of an OPCBrowser object per instance of an OPC Server object. The following properties and methods are included in the OPCBrowser object:
Properties
Methods
Provide Feedback