GetItemID method
Description | Given a name, returns a valid ItemID that can be passed to OPCItems Add method. |
Syntax | GetItemID (Leaf As String) As StringLeaf — The name of a BRANCH or LEAF at the current level. |
Remarks | The server converts the name to an ItemID based on the current "position" of the browser. It will not correctly translate a name if MoveUp, MoveDown, and so on has been called since the name was obtained. |
Example | Dim MyOPCBrowser as OPCBrowser Set MyOPCBrowser = MyOPCServer.CreateBrowser '/* Get item information for this branch MyOPCBrowser.ShowLeafs For i = 1 to MyOPCBrowser.Count '/* Display items at this level lstDisplayItems.Add MyOPCBrowser.GetiItemID(i) Next 'i |
Provide Feedback