ShowLeafs method
Description | Fills the collection with the names of the items at the current browse position. |
Syntax | ShowLeafs (Optional Flat As Variant)Flat — Defines what the collection should contain. If set to True, the collection is filled with all items at the current browse position, as well as all the items in sub branches. If set to False, the collection is filled with all items at the current browse position. |
Remarks | The names of leafs in the collection should match the filter criteria defined by DataType, AccessRights, and Filter. Default for Flat is FALSE. |
Example | Dim MyOPCBrowser as OPCBrowser Set MyOPCBrowser = MyOPCServer.CreateBrowser '/* Get item information for this branch MyOPCBrowser.ShowLeafs |
Provide Feedback