CurrentPosition property
Description | (Read-only) Current position in the tree. This string will be " " (for example, the "root") initially. It will always be " " if Organization is OPCFlat. |
Syntax | CurrentPosition As String |
Remarks | Current Position returns the absolute position and is equivalent to calling GetItemID on a branch. |
Example | Dim MyOPCBrowser as OPCBrowser Set MyOPCBrowser = MyOPCServer.CreateBrowser '/* Display current branch position txtPosition = MyOPCBrowser.CurrentPosition |
Provide Feedback