Organization property

Description
(Read-only) Returns either OPCHierarchical or OPCFlat.
Syntax
Organization
As Long
Remarks
If the organization is OPCFlat, then calling ShowBranches or any Move method has no effect. All names will be available after a single call to ShowLeafs.
Example
Dim MyOPCBrowser as OPCBrowser
Set MyOPCBrowser = MyOPCServer.CreateBrowser
'/* Display browser organization
lblOrganization = MyOPCBrowser.Organization
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal