OPCServer object

The OPCServer object is an instance of an OPC Server. You must create an OPCServer object before you can get references to other objects. It contains the OPCGroups collection and creates OPCBrowser object. The following properties and methods are included in the OPCServer object:
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal