VendorInfo property
Description | (Read-only) Returns the vendor information string for the server. When you access this property, you will get the value that the automation server has obtained from the underlying Data Access Server. |
Syntax | VendorInfo As String |
Remarks | An error occurs if the client has not connected to a Data Access Server via the Connect() method. |
Example | Dim sVendorInfo As String sVendorInfo = MyOPCServer.VendorInfo |
Provide Feedback