GetOPCServers method

Description
Returns the names (ProgID's) of the registered OPC Servers. Use one of these ProgIDs in the Connect method. The names are returned as an array of strings.
Syntax
GetOPCServers
(Optional Node As Variant) As Variant
Node
— String specifying the machine name of the remote node to get the list of registered OPC servers.
Remarks
The use of a node name makes use of DCOM to access another computer. Acceptable node names are UNC names ("Server"), or DNS names ("server.com", "www.vendor.com", or "180.151.19.75").
Example
Dim vAllOPCServers As Variant
'/* Get list of server names
vAllOPCServers = MyOPCServer.GetOPCServers
'/* Add server names to listbox
For i = LBound(vAllOPCServers) To UBound(vAllOPCServers)
lstServers.AddItem vAllOPCServers(i)
Next 'i
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal