OPCGroups collection

The OPCGroups collection is an automation collection containing all of the OPCGroup objects this client has created within the scope of the OPCServer that the Automation Application has connected to via the OPCServer.Connect() The following properties and methods are included in the OPCGroups collection:
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal