DefaultGroupIsActive property

Description
(Read/Write) This property provides the default active state when an OPCGroup is created using the OPCGroups.Add function.
Syntax
DefaultGroupIsActive
As Boolean
Remarks
This property defaults to True.
Example
'/* Set the default group active state to false
MyOPCServer.OPCGroups.DefaultGroupIsActive = False
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal