DefaultGroupUpdateRate property

Description
(Read/Write) This property provides the default update rate (in milliseconds) for an OPCGroup created using the OPCGroups.Add function. This property defaults to 1000 milliseconds (1 second).
Syntax
DefaultGroupUpdateRate
As Long
Example
'/* Set the default group update rate to 250 ms
MyOPCServer.OPCGroups.DefaultGroupUpdateRate = 250
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal