Add method
Description | Creates a new OPCGroup in the OPCGroups collection. |
Syntax | Add (Optional Name As Variant) As OPCGroupName — Optional parameter to give the group a customer specified name. The name must be unique among the other groups created by this client. If no name is provided, the server-generated name will also be unique relative to any existing groups. |
Remarks | If the optional name is not specified, the server generates a unique name. This method will fail if the name specified is not unique. |
Example | Dim WithEvents MyOPCGroup As OPCGroup '/* Add new group to OPCGroups collection Set MyOPCGroup = MyOPCServer.OPCGroups.Add("MyGroupName") |
Provide Feedback