Search
RSLinx Classic Help
Drivers
RSLinx Classic currently supports the following devices:
Manually configured devices
1784-U2DHP driver for DH+ driver
RS-232 DF1 Device configuration
Ethernet device or SoftLogix 5 driver configuration
Ethernet/IP driver configuration
1784-PKTX(D)/PCMK configuration
DF1 Polling Master Driver, General Driver Settings
1784-PCIC(S) configuration
DF1 Slave Driver, General Configuration
DH485 UIC driver
Rockwell Automation Virtual Backplane
DeviceNet drivers
SLC 500 (DH485) Emulator configuration
SmartGuard USB Driver
Remote Devices via RSLinx Gateway configuration
Plug and Play devices
Auto-configured driver for Micro800 series devices
Use drivers and bridge devices
Frequently asked questions (FAQ)
What do I need to purchase to use RSLinx Classic's Ethernet driver?
What steps should I go through to troubleshoot the RSLinx Classic Ethernet driver?
Configure a modem dialer
Auto Configuration Successful
What is a driver?
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal