Remote Devices via RSLinx Gateway configuration
The
Remote Devices via RSLinx Gateway
hardware driver applies to RSLinx Classic Gateway TCP servers. The TCP server functionality of RSLinx Classic Gateway enables RSLinx Classic applications anywhere on an Ethernet TCP network, to reach processor stations on any control network RSLinx Classic Gateway can reach. When you select a Remote Devices via RSLinx Gateway
driver to add or edit, RSLinx Classic opens the Driver Selection
tab on the Configure Remote Devices via RSLinx Gateway
property sheet. Click Browse
to have RSLinx Classic automatically browse your Ethernet TCP network and display the available RSLinx Classic Gateway servers detected.Provide Feedback