Remote Devices via RSLinx Gateway Configure Browser tab
The
Remote Devices via RSLinx Gateway Configure Browser
tab contains the following fields:Network number –
Enter the IP broadcast address for the remote network, which you want to be able to browse to, and then click Add
. This information is available from the network administrator of that network.Networks currently selected for browsing –
The Networks that is currently selected for browsing, list contains those networks that have been added using the Network number data field and the Add
button. These are the networks that will be browsed for RSLinx Classic Gateway servers, in addition to your local network, when you click Browse
on the Driver Selection tab of this dialog box.Provide Feedback