What is a driver?

A driver is the software interface to the hardware device that allows RSLinx Classic to communicate with your PLC. Configuring a software driver is the first step in establishing a DDE hot link.
Select
Communications > Configure Drivers
to open the
Configure Drivers
dialog box that is used for adding, editing or deleting drivers. The available hardware drivers are shown in the Available Driver Types list. The current configured drivers are shown in the
Configured Drivers
list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal