Edit a driver

  1. Select
    Communications > Configure Drivers
    from the RSLinx Classic main menu.
  2. From the
    Configure Drivers
    dialog box, select the desired driver from the Configured Drivers list.
  3. Click
    Configure
    . The configuration dialog box for that driver opens.
  4. Make the necessary modifications to the driver, and click
    OK
    to return to the
    Configure Drivers
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal