DDE/OPC Topic Configuration

In RSLinx Classic, a topic represents a specific path to a processor. If you right-click a station in
RSWho
and select
Configure DDE Topic
, or if you select
DDE > Topic Configuration
, the
DDE/OPC Topic Configuration
dialog box opens.
A DDE project is a storage container for one or more DDE topics. If you attempt to create a DDE topic without having created a DDE project, a default DDE project is created for you.
If you selected
Configure DDE
Topic by right-clicking on a station in
RSWho
, the Topic Name box is pre-filled. RSLinx Classic starts with the name of the program running in the processor, and if this DDE topic exists, it adds a number to the end until it finds one that does not exist. If there are any spaces, it converts them to _'s. You can change the topic name RSLinx Classic selected for you.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal