Edit a topic
- SelectDDE/OPC > Topic Configurationfrom the RSLinx Classic main menu.
- From theDDE/OPC Topic Configurationdialog box, select the DDE topic you want to edit from theTopic List.
- Make the necessary modifications to the topic and clickApply.
- ClickYeswhen prompted with the message "Are you sure you want to update topic (topic_name)?"
- When you are finished adding topics, clickDoneto close theDDE/OPC Topic Configurationdialog box.TIP:After selecting the topic to edit from theTopic List, you can also right-click to Rename, Clone, or Delete the topic.
Provide Feedback