DDE
Dynamic Data Exchange (DDE) is a standard inter-application communication protocol built into Microsoft Windows operating systems and supported by many applications that run under Windows. DDE takes data from one application and gives it to another application. It allows Windows programs that support DDE to exchange data between themselves.
- ADDE serveris a program that has access to data and can provide that data to other Windows programs.
- ADDE clientis a program that can obtain data from a server.
By specifying an application, topic, and item, a client application can exchange data with a server application.
DDE works like a conversation between two people. The people represent the different applications running under Windows, and the data they share is what they are talking about.
Applications using DDE to talk to RSLinx Classic do not care what kind of data they are getting. All they know is there is a DDE link, and that link is providing data. What that data is and how it will be used is immaterial to the receiving application.
For example, if you have a DDE link from RSLinx Classic to an Excel spreadsheet, Excel does not know that you are sending a counter value into a spreadsheet. All Excel sees is data.
For example,
RSLINX
is the application name, PLC5TOPIC1
is an example topic name, and C5:0.ACC
is an example item, in this case a counter accumulator in an Allen-Bradley PLC-5.
TIP:
Not all applications that run under Microsoft Windows support DDE. Check with an application's manufacturer before purchasing an application for use with RSLinx Classic.
Provide Feedback