Application

When you use a Windows NT application to obtain data from another Windows NT application, you must provide the name of the application you want to respond to your message. When you use a DDE link between two applications, you specify the name of the application you want to exchange data with. For example, if you want to send data to a Microsoft Excel spreadsheet, the application name is EXCEL (for the Excel version 5.0 format). When you ask RSLinx Classic for data, the application name to use is RSLINX.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal