Endpoints

How do I open Endpoints?
  1. From the
    Start
    menu, select
    Rockwell Software > FactoryTalk Linx Gateway Configuration
    .
  2. Expand
    OPC UA Server
    , and the select
    EndPoints
    .
Use
Endpoints
to add, remove, and configure
OPC
UA server endpoint URLs and properties.
Endpoints
Field
Description
Add
Delete
Name
Shows the name for the
OPC
UA server endpoint. The name must be unique. The server name displays in the
OPC
UA namespace and is included in the full tag path for all nodes provided by the server.
URL
Shows the network path to the
OPC
UA Server.
Security Policy
Displays whether security is required or optional for connections between
OPC
UA clients and the
FactoryTalk Linx Gateway
OPC
UA server.
Security Mode
Displays the security method required for connections between
OPC
UA clients and the
FactoryTalk Linx Gateway
OPC
UA server.
Endpoint Properties
Field
Description
Name
Sets the name for the
OPC
UA server endpoint. The name must be unique. The server name displays in the
OPC
UA namespace and is included in the full tag path for all nodes provided by the server.
Address
Selects the hostname or IP address of the computer.
Port
Sets the port number for the
OPC
UA server endpoint. The port must be unique. The default port is 4990 and increments by 1 for each additional endpoint.
The firewall on the
FactoryTalk Linx Gateway
OPC
UA server must allow incoming connections to the selected port for the connection to succeed.
URL
Gets the network path to the
OPC
UA Server.
This URL must be provided to
OPC
UA client applications in order to connect to the
FactoryTalk Linx Gateway
UA service.
Copy
Copies the URL into the windows clipboard, so it can be pasted into the OPC UA Client.
Disable
Turns off the endpoint.
Enable reverse connect
Enables a server to initiate the connection to an OPC UA client.
  • Client URL
Sets the URL to identify the OPC UA client the server will communicate with using the reverse connect.
The URL must be in the format
opc.tcp://hostname_or_ip:port/Endpoint
where
hostname_or_ip
and
port
are replaced with the hostname or IP address and port number of the OPC UA client.
Endpoint
is optional. Do not use the port that is already occupied by other clients.
The maximum number of Client URLs supported is 20 for each endpoint. It is available when configuring reverse connect.
  • Max Connection
Sets the maximum number of clients connected to the current UA server endpoint. These clients should be on the same computer with the same client URL.
The valid range of Max Connection is from 1 through 20. It is available when configuring reverse connect.
Anonymous
Grants the
Anonymous
account with access to
FactoryTalk Linx Gateway
.
Limit to read-only access
Sets
Anonymous
account with only read access.
Enable read access to CIA message
Permits an OPC UA client connected to
FactoryTalk Linx Gateway
with Anonymous login and read access permissions to retrieve information from a device using a
FactoryTalk Linx
shortcut configured with: CIP Object - Class/Instance/Attribute Message
Enable write access to CIA message
Permits an OPC
UA client connected to
FactoryTalk Linx Gateway
with Anonymous login and write access permissions to send information to a device using a
FactoryTalk Linx
shortcut configured with: CIP Object - Class/Instance/Attribute Message
FactoryTalk Security User
Sets FactoryTalk Security user with read and write access. The user is created in
FactoryTalk Administration Console
> System > Users and Groups. Username and password are needed.
Security Policy
Displays whether security is required or optional for connections between
OPC
UA clients and the
FactoryTalk Linx Gateway
OPC
UA server.
There are four security algorithm suites:
  • None
  • Basic128Rsa15
    The OPC UA specification deprecated this option. We don't recommend it.
  • Basic256
    The OPC UA specification deprecated this option. We don't recommend it.
  • Basic256Sha256
  • Aes128Sha256RsaOaep
  • Aes256Sha256RsaPss
Security Mode
Displays the security method required for connections between
OPC
UA clients and the
FactoryTalk Linx Gateway
OPC
UA server.
  • Sign:
    Use signature to secure the connection.
  • Sign & Encrypt:
    Use signature and encryption to secure the connection.
  • Sign + Sign & Encrypt:
    Use either signature or signature and encryption to secure the connection.
Log diagnostic message on tag write
When enabled,
FactoryTalk Linx Gateway
will create a diagnostic or audit message every time a tag is written by an external
OPC
UA client. The default setting is disabled.
Log as audit message
When enabled,
FactoryTalk Linx Gateway
will create an audit message in the FactoryTalk Audit log with time-and date-stamped information to track changes that occurred during the operation of the system.
Log as diagnostic message
When enabled,
FactoryTalk Linx Gateway
will create a diagnostic message in the FactoryTalk Diagnostics log with time-and date-stamped information to help diagnose anomalies.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal