Authenticate an OPC UA client
FactoryTalk Security
secures the automation system by limiting access to those with a legitimate need. Use FactoryTalk Security
to limit an OPC
UA client to access data through FactoryTalk Linx Gateway
.There are two ways of logging on
FactoryTalk Linx Gateway
service:- Anonymous
- FactoryTalk Security User
By default, the OPC UA client logs on
FactoryTalk Linx Gateway
service using Anonymous
logon, which means no username or password is needed. And the OPC UA client has full access of browsing, reading, and writing data through FactoryTalk Linx Gateway
.To log on using FactoryTalk Security User
- InFactoryTalk Linx GatewayConfiguration, expandOPC UA Server, and then selectEndPoints.
- OnEndpoint Properties, underAuthentication Settings, select FactoryTalk Security User.You cannot select None as the Security Policy if you want to logon using FactoryTalk Security User
- Go toFactoryTalk Administration ConsoleorFactoryTalk View StudioExploretopology tree, expandSystem>Users and Groups.
- Right-clickUsers, and then clickNew>FactoryTalk User...
- Enter username and password, and then clickOK.For more information about New User properties, seeFactoryTalk Services Platform Help.
- Set permissions for the newly added user to perform certain actions.
- Go to OPC Client, connect toFactoryTalk Linx Gatewayby selecting the same security policy configured inFactoryTalk Linx Gatewayserver.
- Enter theFactoryTalk Securityusername and password, and then connect toFactoryTalk Linx Gatewayserver.
Provide Feedback