Feature Security Properties

Use the
Policy Settings
tab in
Feature Security Properties
dialog box to secure features of a single
FactoryTalk
product. By setting permissions to a single feature, you can limit a user or a group of users to perform securable actions.
FactoryTalk Linx Gateway
supports the user security by requesting the users to log on to
FactoryTalk Linx Gateway
server when starts
FactoryTalk Linx Gateway
Configuration and when changing the scope.
The logon scope is determined by the user's activation type. If a user has a local license, he can only log on to local scope. If the user has a network license, he can logon to both network and local scope.
To log on
FactoryTalk Linx Gateway
server, do one of the followings:
  • In the
    Log On to FactoryTalk
    dialog, enter the username and password.
    TIP:
    • If you have enabled single sign-on function in
      FactoryTalk Services Platform
      >
      Explorer
      >
      System Policies
      >
      Security Policy
      , there is no need to manually log on
      FactoryTalk Linx Gateway
      server.
    • Log off and log on back for the feature security settings to take effect.
As the product policy is configured upon the logon scope, make sure the
FactoryTalk Linx Gateway
server logon scope is the same with
FactoryTalk Diagnostics
scope.
The following table shows the relationship between
FactoryTalk Linx Gateway
feature security policies and securable actions that the user can perform:
Feature security policy
Description
View Gateway Server Properties
Allow users to view information on
Global Settings
and the settings on interfaces.
Modify Gateway Server Properties
Allow users to modify information on
Global Settings
and the settings on interfaces.
View Tag List Configuration
Allow users to view information on
UA Tag List
.
Modify Tag List Configuration
Allow users to modify settings on
UA Tag List
.
View UA Server Endpoint Properties
Allow users to view UA server configuration information and security settings on
Endpoints
including the endpoints.
Remove UA Server Endpoint
Allow users to remove the selected endpoint on
Endpoints
.
Add/Configure UA Server Endpoint Properties
Allow users to add a new endpoint and edit existing endpoints' configuration information and security settings on
Endpoints
including.
Manage Incoming Certificate
Allow users to view and import, reject, trust and remove certificates in
OPC UA Server >
Certificate Management > Incoming Certificate
.
View Outgoing Certificate Properties
Allow users to view the outgoing certificates information in
OPC UA Server >
Certificate Management
>
Outgoing Certificate
.
Modify Outgoing UA Certificate Properties
Allow users to regenerate an outgoing certificate when the old one is expired or there is a need to do so.
OPC UA Client Read Access
Allow OPC UA clients to read data values through
FactoryTalk Linx Gateway
server.
OPC UA Client Write Access
Allow OPC UA clients to read and write data values through
FactoryTalk Linx Gateway
server.
CIA Message Client Read Access
Allow OPC UA clients to read CIA message through FactoryTalk Linx Gateway server.
CIA Message Client Write Access
Allow OPC UA clients to read and write CIA message through FactoryTalk Linx Gateway server.
View Custom UA Namespace
Allow users to view information on
Custom Namespace
of
OPC UA Server
.
Modify Custom UA Namespace
Allow users to edit configurations on
Custom Namespace
of
OPC UA Server
.
View MQTT Configuration
Allow users to view the MQTT configurations.
Modify MQTT Configuration
Allow users to edit the MQTT configurations.
View Custom RTD/DDE Namespace
Allow users to view information in
Custom Namespace
of
RTD Server
and
DDE Server
.
Modify Custom RTD/DDE Namespace
Allow users to edit information on
Custom Namespace
of
RTD Server
and
DDE Server
.
View Remote Proxy Service
Allow users to view information on
Remote Proxy Service
.
Modify Remote Proxy Service
Allow users to edit on
Remote Proxy Service
.
View SDK Interface
Allow users to view information on
Linx SDK Interface
.
Modify SDK Interface
Allow users to edit configurations on
Linx SDK Interface
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal