Secure FactoryTalk Linx Gateway with FactoryTalk Security
FactoryTalk Security
secures the automation system by limiting access to those with a legitimate need. Use FactoryTalk Security
to authenticate user identities and authorize user requests to access a FactoryTalk
-enabled system. These security services are fully integrated into the FactoryTalk Directory
as part of the FactoryTalk Services Platform
that installs with many products.
TIP:
If you prefer not to use security services, grant all users full access to your automation system.
To secure
FactoryTalk Linx Gateway
with FactoryTalk Security
Provide Feedback