Configure Reverse Connect
Usually, a connection is opened by the client before starting the UA-specific handshake. However, this will fail when servers are behind firewalls with no open ports to connect to. In the reverse connectivity scenario, the server opens the connection and starts with a ReverseHello message requesting that the client establish a secure channel using this connection.
To use
Reverse Connect
, you should configure the connection in both FactoryTalk Linx Gateway and the OPC UA client.
IMPORTANT:
Changing the Max Connection to 1 may prevent client communication because some OPC UA clients require 2 connections to operate normally.
To configure Reverse Connect in FactoryTalk Linx Gateway
- InEndpoint Properties, selectEnable reverse connect.
- ClickAdd.
- InReverse Connect, enter the client URL.The URL must be in the formatopc.tcp://hostname_or_ip:port/Endpointwherehostname_or_ipandportare replaced with the hostname or IP address and port number of the OPC UA client.Endpointis optional. Do not use the port that is already occupied by other clients.Example: client IP=192.168.1.1, port number=4001, Client URL= opc.tcp://192.168.1.1:4001
- SelectSave.
For more details about Reverse Connect, see Endpoints.
To configure Reverse Connect in UA Client (taking UaExpert as an example)
- In theUnified Automation UaExpertdialog box, click
to add a server. - In theAdd Serverdialog box, underReverse Discovery, enter the URL that is the same URL entered in theClient URLbox in FactoryTalk Linx Gateway.
- ClickOK.
Provide Feedback