Delete an OPC UA server endpoint
Delete an
OPC
UA server endpoint so OPC
UA clients can no longer connect to FactoryTalk Linx Gateway
through its URL. A minimum of one OPC
UA endpoint is required per FactoryTalk Linx Gateway
UA server.To remove an
OPC
UA server endpoint- From theStartmenu, selectRockwell Software >.FactoryTalk Linx GatewayConfiguration
- UnderOPC UA Server, selectEndPoints.
- Select the server endpoint to remove, and then selectDelete.
- SelectOK.
Provide Feedback