Standalone Data Service

  1. From the
    Start
    menu, select
    Rockwell Software
    >
    FactoryTalk Linx Gateway Configuration
    .
  2. Select
    Global Settings
    , under
    Data Source
    , select
    FactoryTalk Linx Gateway Standalone Data Service
    .
Standalone Data Service
supports data acquisition from Logix 5000 controllers version 18 and later using the
FactoryTalk Linx Gateway
. The
Device shortcut configuration
pane and the FactoryTalk Linx Network Browser within FactoryTalk Linx Gateway allow you to use the
FactoryTalk Linx Gateway Standalone Data Service
without creating FactoryTalk applications and FactoryTalk Linx servers. Distributed applications and redundant FactoryTalk Linx servers are not supported.
The following table shows the supported namespace modes of each server using the standalone data service.
Interface
Folder with scalar data
Tag list and structures/array access
Custom namespace
OPC UA Server
No
No
Yes
MQTT
No
No
Yes
OPC DA Server
Yes
No
No
RTD Server
Yes
No
Yes
DDE Server
Yes
No
Yes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal