Items in the Network Browser pane
The items in the Network Browser pane are listed in the following table.
Field | Description |
|---|---|
![]() | Adds the device path to the shortcut. |
![]() | Determines whether to enable the Network Browser to discover the selected device or network branch continuously. |
![]() | Increases or decreases the view of the network topology tree. |
![]() | Filters a list of devices with the search criteria. |
![]() | Opens Advanced Settings to configure network discovery settings. |
![]() | Adds a driver on the computer to provide communications to a network and configures existing drivers. You can add or configure Ethernet drivers. |
For more information, see
FactoryTalk Linx Network Browser
in FactoryTalk Linx Help
.
TIP:
The configuration changes made to drivers in the network browser pane are shared with the standalone FactoryTalk Linx Network Browser launched from the Windows Start menu.
Provide Feedback