Items in the Device shortcut configuration pane

The items in the
Device shortcut configuration
pane are listed in the following table.
Field
Description
Adds a shortcut.
Deletes the selected shortcuts at a time.
Filters the shortcuts with the search criteria.
Shortcut Name
Edits the shortcut name.
Type
Selects the shortcut type. Only the Processor type is supported, and it can only point to a Logix Controller.
Path
Edits the device path. You can enter the path or select a device from the Network Browser.
Count
Shows the number of shortcuts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal