Items in the Properties pane

The items in the
Properties
pane are listed in the following table.
Field
Description
Shortcut Name
Edits the shortcut name.
Description
Edits the description for the shortcut.
Type
Selects the shortcut type. Only the Processor type is supported.
Path
Edits the device path connected to the shortcut.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal