User Settings

User Settings

Perform the following steps to change the language details:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    User Settings
    .
    The User Settings page is displayed.
  2. Click
    Edit
    .
  3. Select the required language (English or Spanish) from the
    Default Language
    drop-down list.
    NOTE: By default, English language is selected.
  4. Click
    Save
    .
    User Settings
NOTE: All labels, static text, and static tooltip are changed to the configured language.
Dashboard in Spanish Language
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal