User interface
- InFactoryTalk Administration ConsoleExplorer, expand an application or area, right-click an OPC UA Connector, and then selectProperties.
Use the dialog box to add or edit
FactoryTalk Linx
OPC
UA ConnectorFactoryTalk Linx
OPC
UA Connectors or add, edit, or remove OPC
UA Servers.The dialog box consists of the following tabs:
FactoryTalk Linx
OPC
UA Connector- Connector Settings
- Redundancy
- OPC UA Servers
- Certificate Management
- Real Time Diagnostics
- FactoryTalkDiagnostic Log
- About
TIP:
New features supported for
FactoryTalk Linx
OPC
UA Connector in FactoryTalk Services Platform
version 6.10.00 and later cannot be configured or used by computers running FactoryTalk Services Platform
version 3.00.00. To use these features, update all computers used to host or configure FactoryTalk Linx
OPC
UA Connector to FactoryTalk Services Platform
version 6.10.00 or later.Provide Feedback