Certificate Management

  1. In
    FactoryTalk Administration Console
    , right-click an OPC UA Connector, and then select
    Properties
    .
  2. In , select
    Certificate Management
    .
Use
Certificate Management
to view and manage
FactoryTalk Linx
OPC UA Connector and OPC UA Server security certificates.
When an OPC UA Connector begins communication with an OPC UA Server, the OPC UA Connector provides the OPC UA Server with its security certificate. The OPC UA Server accepts or rejects the certificate to authorize or deny communication to the OPC UA Connector. Security certificates may be required for some OPC UA Servers.
FactoryTalk Services Platform
creates a default, self-signed security certificate during installation. The certificate is stored at
C:\ProgramData\Rockwell\OpcUaConnector\RnaUaClientDataProvider\PKI\own\
on the computer hosting
FactoryTalk Linx
OPC UA Connector.
If a security certificate signed by a trusted security authority is required, replace the default security certificate with the required certificate. A custom security certificate must have the same name and file path as the default security certificate.
FactoryTalk Linx
OPC
UA Connector version 6.20.00 or later supports creating a Certificate Signing Request (CSR) to obtain a new certificate from an external signing authority.

Certificate Properties

General
Property
Description
Name
Displays the name of the security certificate.
Status
Displays the certificate status, either
Trusted
or
Rejected
.
Certificate
Property
Description
Location
Displays the path to the security certificate on the
FactoryTalk Linx
OPC
UA Connector computer.
Application Name
Displays the application from where the certificate is presented.
Organization
Displays the organization name that was submitted to CA when requesting the certificate.
Application URI
Displays the
FactoryTalk Linx
OPC
UA Connector application URI associated with the security certificate.
Domain
Displays the workstation name.
Subject Name
Displays the subject properties on the certificate. For example, Common Name (CN).
Valid From
Displays the date and time when the security certificate is valid.
Expiration Time
Displays the date and time when the security certificate expires.
Thumbprint
A short sequence of bytes created by applying the cryptographic hash function to identify a certificate.

Incoming Certificate

Trusted Certificates
Button
Description
Import
Specifies and imports the certificate to be used as an incoming certificate.
Reject
Moves the specific certificates from the
Trusted Certificates
list to the
Rejected Certificates
list. The servers cannot communicate with
FactoryTalk Linx
OPC
UA Connector.
Remove
Removes the specific certificates from the
Trusted Certificates
list. The servers cannot communicate with
FactoryTalk Linx
OPC
UA Connector.
Rejected Certificates
Button
Description
Trust
Adds the specific certificate to the
Trusted Certificates
list. The server can communicate with
FactoryTalk Linx
OPC
UA Connector.
Remove
Removes the specific certificates from the
Rejected Certificates
list. The servers cannot communicate with
FactoryTalk Linx
OPC
UA Connector.

Outgoing Certificate

Button
Description
Create CSR
Creates a certificate signing request and saves the request as a CSR file.
Import
Specifies and imports the certificate to be used as an outgoing certificate.
Regenerate
Creates another certificate to renew the valid period.

Others

Button
Description
Refresh
Refreshes to display the latest certificates.
Manage Access
Limits access to security certificate management operations to administrators or individuals approved by an administrator. This function is only available to Administrator.
If you are an Administrator and in the Administrator group, but this option is still not available, do the following:
1. In
Run
, enter
gpedit.msc,
and then select
OK
.
2. In
Local Group Policy Editor
, select
Computer Configuration
>
Windows Settings
>
Security Settings
>
Local Policies
>
Security Options
.
3. Double-click
User Account Control: Run all administrators in Admin Approval Mode
.
4. Select
Disabled
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal