FactoryTalk Diagnostic Log
- InFactoryTalk Administration ConsoleExplorer, right-click an OPC UA Connector, and then selectProperties.
- InFactoryTalk Linx OPC UA Connector, selectFactoryTalk Diagnostic Log.
Use
FactoryTalk Diagnostic Log
to view historical error, warning, and information diagnostic messages about the OPC UA Connector on the local computer. The information shown is limited to the selected OPC UA Connector and the connected OPC UA Servers.Button | Description |
---|---|
Refresh | Clears FactoryTalk Diagnostic Log and refreshes diagnostic messages from the FactoryTalk Diagnostics server on the local computer. |
Launch FactoryTalk Diagnostic Viewer | Starts FactoryTalk Diagnostic Viewer to view diagnostic messages for all FactoryTalk devices and services or view diagnostic messages for a remote computer. |
Provide Feedback