View logged diagnostics
Use
FactoryTalk Diagnostic Log
to view historical error, warning, and information level diagnostic messages about the OPC UA Connector on the current computer.
TIP:
To view diagnostic messages about an OPC UA Connector hosted on a remote computer, perform one of the following actions:
- Use theFactoryTalk Administration ConsolehostingFactoryTalk LinxOPC UA Connector on the computer.
- Select and configureLaunch FactoryTalk Diagnostic Viewerto view logs from the computer hostingFactoryTalk LinxOPC UA Connector.
To view logged diagnostics for an OPC UA Connector
- InFactoryTalk Linx OPC UA Connector, selectFactoryTalk Diagnostic Log.
Provide Feedback