About

  1. In
    FactoryTalk Administration Console
    , right-click an OPC UA Connector, and then select
    Properties
    .
  2. In , select
    About
    .
Use
About
to identify the version of the
FactoryTalk Linx
OPC
UA Connector user interface and
FactoryTalk Linx
OPC
UA Connector service.
Field
Description
Configuration User Interface Revision
Lists the version number of the
FactoryTalk Linx
OPC
UA Connector user interface on the local machine.
FactoryTalk Linx
OPC UA Connector Revision
Lists the version number of the
FactoryTalk Linx
OPC
UA Connector service. Depending on the network configuration, the OPC UA Connector might be on a remote machine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal