Configure the Alarm and Event Summary
The
Alarm and Event Summary Properties
dialog box contains tabs that are used to configure the appearance and operation of the Alarm and Event Summary object at runtime:- Appearance. Use theAppearancetab to change how information is displayed and how users interact with the information.
- Columns. Use theColumnstab to change which columns are displayed and to configure their appearance.
- Toolbar. Use theToolbartab to change the buttons that appear on the toolbar.
- Status Bar. Use theStatus Bartab to select the items that are displayed in the status bar and to change their order.
- Event Subscriptions. Use theEvent Subscriptiontab to subscribe to events that match defined criteria.
- Display Filters. Use theDisplayFilterstab to limit the data displayed based on defined criteria.
- Sort. Use theSorttab to sort the data displayed on the contents of different fields.
- States. Use theStatestab to configure a distinct appearance for each of the alarm states and alarm priorities.
- Behavior. Use theBehaviortab to control how operators can interact with the Alarm and Event Summary at runtime.
Provide Feedback