Methods (AlarmBanner)
The following table lists the information about the methods.
Methods—AlarmEventBanner object | |
---|---|
AckSelected | Acknowledges the selected alarm. |
AckSelectedWithComment | Acknowledges the selected alarm. Optionally, a dialog box is displayed. Operators can use the dialog box to enter a comment, or a comment can be entered programmatically. |
MoveSelectionDown | Moves the selection one item down in the event list. |
MoveSelectionUp | Moves the selection one item up in the event list. |
RunAlarmCommand | Runs the alarm command that is associated with the selected alarm specified in the Alarm and Event Banner configuration. |
RunSummaryCommand | Runs the Alarm and Event Summary command. |
SilenceAll | Silences the audible notifications associated with the alarms in the Alarm and Event Banner. The bell stops ringing until a new alarm triggers it. |
ShelveSelected | Shelves the selected alarm with the specified duration. |
Provide Feedback