Alarm and Event Banner object model

Use the FactoryTalk® Alarm and Event Banner object to subscribe to alarms from one or more areas in the FactoryTalk system and then monitor and interact with the most urgent and recent alarms.
The Alarm and Event Banner can:
  • Display various attributes of alarms.
  • Indicate the state of alarms using icons, colors, and sound.
  • Be used by operators to acknowledge or silence the alarms that are displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal