Properties (AlarmBanner)
The following table lists the information about the properties.
Properties—AlarmEventBanner object | |
---|---|
AlarmBellActive | Returns a value indicating whether the alarm bell is active. |
AlarmBellEnabled | Sets or returns a value indicating whether the alarm bell is enabled. |
AlarmFaultCount | Returns the number of alarm faults. |
InAlarmAckedCount | Returns the number of In Alarm and Acknowledged alarms. |
InAlarmUnackedCount | Returns the number of In Alarm and Unacknowledged alarms. |
MaintainSelection | Sets or returns a value indicating whether the selection in the event list is maintained when the object loses focus. |
NormalUnackedCount | Returns the number of Normal and Unacknowledged alarms. |
SelectedEvent | Returns an EventItem object representing the event that is currently selected in the event list. |
Provide Feedback