AlarmBanner object
The AlarmEventBanner is the root object of the Alarm and Event Banner and represents an instance of the Alarm and Event Banner. The AlarmEventBanner object is accessible from the container hosting the AlarmEventBanner object.
Provide Feedback