MoveSelectionUp method

Moves the selection one item up in the event list. If the selected item is at the top of the list, the selection is not moved.
Syntax
object
.
MoveSelectionUp
where
object
the name of an AlarmEventBanner object.
To use buttons on a FactoryTalk View graphic display that call this method, the Alarm and Event Banner must be configured to
Maintain selection when focus lost
for the method to function. If the
Maintain selection when focus lost
is not selected then the selected row is lost when the button is clicked.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal