AckSelected method
Acknowledges the selected alarm.
Syntax
object
.AckSelected
where
object
—the name of an AlarmEventBanner object.Possible errors
- ftasErrorServerConnectionLost
- ftasErrorInsufficientRights
- ftasErrorGeneralFailure
- ftasErrorUnknownAlarm
- ftasErrorOperationIgnored
To use buttons on a FactoryTalk View graphic display that call this method, the Alarm and Event Banner must be configured to 'Maintain selection when focus lost’ for the method to function. If the 'Maintain selection when focus lost’ is not selected, then the selected row is lost when the button is clicked.
Provide Feedback