MoveSelectionDown method
Moves the selection one item down in the event list. If the selected item is at the bottom of the list, the selection is not moved.
Syntax
object
.MoveSelectionDown
where
object
—
the name of an AlarmEventBanner object.To use buttons on a FactoryTalk View graphic display that call this method, the Alarm and Event Banner must be configured to
Maintain selection when focus lost
for the method to function. If the Maintain selection when focus lost
is not selected then the selected row is lost when the button is clicked.Provide Feedback