ShelveSelected method
Shelves the selected alarm with the specified duration.
Syntax
object
.ShelveSelected
([ShowDialog
as Boolean
], [Comment
as String
], [IShelveDuration
as Long
])where
object
—
the name of an AlarmEventBanner object.ShowDialog
—
optional parameter that controls whether the Shelve Alarm
dialog box is displayed before the selected alarm is shelved.- TRUE. The default value is TRUE. If ShowDialog = TRUE, then theShelve Alarmdialog box opens and offers users the possibility of entering a comment and duration before the alarm is shelved.
- FALSE. If ShowDialog = FALSE, then theShelve Alarmdialog box is NOT displayed before the alarm is shelved. The selected alarm is shelved using the value of theCommentandIShelveDurationparameters.Comment—optional parameter that controls the comment string associated with the alarm shelving.IShelveDuration—optional parameter that controls the duration associated with the alarm shelving. The default value is 1. The value must be between 1 and 2147483647.
Provide Feedback