User Group Properties

How do I open User Group Properties?
  1. In the
    Explorer
    window, expand the
    FactoryTalk
    network or local directory tree, and then expand the
    System
    folder until the user group account you want to modify is visible.
  2. Right-click the user group account, and then click
    Properties
    .
For a
FactoryTalk
user group account, use
User Group Properties
to edit the name, description, and email account associated with the user group account, and to add or remove users from the group.
For a
Windows
-linked user group and an LDAP-linked user group, these properties are viewable. Use
Change Domain
to link this user group account to a different
Windows
domain
.
Setting
Description
Name
Type a name for the user group.
Description
(optional) Enter information about the group, such as the group location, relevant parts of the system to the group, or contact information.
E-mail
(optional) Type one email address or group address, (for example
cjenkins@yourcompany.com
or
maintenance@yourcompany.com
), to associate with this account.
Members
Lists the current members of the group. Add or remove members from this list in a
FactoryTalk
user group account
. To change the membership of a
Windows
-linked user group, use
Windows
.
Add
Remove
Change Domain
Visible only in a
Windows
-linked user account. Select
Change Domain
to move the
Windows
-linked user group to a different domain.
Changes to a user's group memberships take effect when the user logs off
FactoryTalk
and then logs on again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal