Move a Windows-linked user group to a different domain
Windows
-linked user group accounts, and the user accounts they contain, can move from one domain to another while keeping security permissions for the group accounts intact. Delete individual Windows
-linked user accounts and recreate the accounts in the new domain. This causes all security permissions for the user accounts to be lost.
TIP:
Moving
Windows
-linked user group accounts to a new domain in one directory does not move them in the other. To move the accounts in both directories, move them in one directory then log off that directory. Log on to the other director, and then move them in the second directory.Prerequisites
Obtain these permissions in the
User Groups
folder in FactoryTalk Administration Console
Explorer
:- Common > List Children
- Common > Read
- Common > Write
To move a
Windows
-linked user group to a different domain- In the newWindowsdomain, create a user group with the same name as the one currently linked in theFactoryTalksystem. For details, seeWindowsHelp.
- InFactoryTalk Administration ConsoleExplorer, expandSystem>User Groups, right-clickWindows-linked user group, and selectProperties.
- InGeneral User Group Properties, selectChange Domain.
- InSelect, select the target domain for theWindowsDomainWindows-linked user group, selectOK.The new domain must already contain a user group with the same name as the user group in the old domain, otherwise cannot move the group.
- InUser Group Properties, selectOK.
Provide Feedback